AXIS#.MOTIONDISSOURCES
Description
AXIS#.MOTIONDISSOURCES is a bit-field that returns some of the reasons that motion may not be allowed on the axis. There are additional reasons why the drive cannot accept a motion command that are not reported by this command (for example, fieldbus control bits or fault status).
| Bit | Description |
|---|---|
| 0 | The axis is disabled (see AXIS#.ACTIVE). |
| 1 |
Controlled stop and stay enabled is active. This bit could be set for several reasons:
|
| 2 | One or both of the brakes are not released if brakes are configured on this axis. |
| 3 | Rotor flux not ready. Only applicable for induction motors (see AXIS#.MOTORTYPE). |
| 4 | Wake and Share active (see AXIS#.WS.STATE ). |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Bit 4 added | 02-02-05-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer (bit-field) |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics